This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24030: How to shutdown the output of BQ24030?

Part Number: BQ24030


I want to shut down the output current of BQ24030 by setting CE pin low. It works fine when the power is from AC or USB. However, when it is powered with a battery, the CE pin cannot shut down the output. I found in the datasheet which says " The bqTINY III- series enters the low-power standby mode when the CE input is low with either AC or USB present ". Does this mean there is no way to shut down the system when powered with the battery?