Hi sirs,
We test the VNN(Vgfx) dynamic VID measurement.
test condition:
Vmax | 1.150 V |
Vmin | .950 V |
Static Icc | 0 A |
SVID Dn | Slow |
SVID Up | Fast |
High PS | 0 |
Low PS | 2 |
Voltage change 5us after ALERT to settled is 19mV.
It over spec. 11.3mV.
The change of Dynamic VID is too slow.
So I change Rcomp(R363) from 11K to 13.3K
The Dynamic VID is pass.
Is there any bad influence for this design R363 change to 13.3Kohm?
Please help to confirm.
Thanks.2211.tps59641.pdf