This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULQ2004A: power consumption of the package

Part Number: ULQ2004A

Hi,staff

ULQ2004ADR

Please tell me the allowable power consumption of the package
best regards
cafain
  • Hi cafain

    The abs max junction temp is 150C and I assume this is being run in 25C ambient.

    Using the R_theta,j,a for the D package on the datasheet, I calculated that the maximum power dissipation is around 1.7W.

    Limiting the power dissipation to 1.5W will guarantee safe and reliable operation of the device.