Other Parts Discussed in Thread: BQ76930
I have a board with a BQ76920, and external balancing circuit that was designed after http://www.ti.com/lit/ug/slvu925c/slvu925c.pdf
When setting balancing bits, and reading back the register to confirm that the bits are set, there is no apparent difference in current being drawn from that cell (scoping 1 ohm shunt) even though we should see between a 30-40 mA increase. Upon further probing, the FET never appears to be set. The source-drain voltage is that of the cell, and the gate voltage was about equal to the source voltage. This stayed steady as the balance bit for the corresponding flipped on and off.