Other Parts Discussed in Thread: TPS63802
Hello,
how much is the power consumption (µA) from TPS63001 voltage regulator in shutdown mode?
We need this Information before we start an battery powered project.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Christian,
The input current in shutdown mode is 0.1 µA typical and 1 µA maximum for the TPS63001, as shown in the datasheet.
If low power consumption is your main requirement, you might also take a look at the TPS63802. It is a similarly specified device, but with lower Isd and Iq, therefore more suitable for battery powered applications.
Best regards,
Milos