I am performing the DS Calculations Page 27. I need all information required to perform these calculations. Below are my questions.
Reference DS Equations 30 thru 33, Page 27.
Unknown Term “K3rd”, Is this the third harmonic for 60 Hz which would be 180 Hz?
Question 1) Define the unknown term “K3rd”.
Question 2) Is “K3rd” a constant? {Yes or No} If yes, what is the constant value used.
Question 3) Is “K3rd” a variable? {yes or No} If yes:
-
What is the min/max value.
-
What are the Test Conditions used to determine these values.
Question 4) Is there any information that is required to determine the correct value of “K3rd” that I have not asked.
Unknown Term “Gmv”, Is this the value listed in DS Page 6, 5th line from bottom, (70uS)?
Question 5) Define the unknown term “Gmv”.
Question 6) Is “Gmv” a constant? {Yes or No} If yes, what is the constant value used.
Question 7) Is “Gmv” a variable? {yes or No} If yes:
-
What is the min/max value.
-
What are the Test Conditions used to determine these values.
Question 8) Is there any information that is required to determine the correct value of “Gmv” that I have not asked.