Other Parts Discussed in Thread: TPS40210
Tool/software: WEBENCH® Design Tools
Hi,
We are considering LM5022 at SEPIC topology with the following conditions.
Vin=10V~36V, Vo=12V, Io=3A
At the beginning of the considering , we simulated at WEBENCH. However the inductor was larger than expected.(180uH)
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=B8169160B99CC2C5
On the other hand, we tried another device such as TPS40210. The inductor was small.(15uH)
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=FDE86F61BF93777A
Why is the indcutor different with LM5022 and TPS40210?
I understand the inductor is depended on the switching frequency.In the case of LM5022 , the freq is 100kHz. In the case of TPS4021, it was 370kHz.
(We tried to change the freq of LM5022. But it couldn't ) Why the value is so different between LM5022 and TPS40210? What kind of parameter or spec of the device is related ?
Best Regards,
Koji Hamamoto