Hello,
what is the maximum continuous output current of the LM3410? I would like to power it from 5V power supply and connect one 12V LED with 1A. Is LM3410 able to handle it?
Thank you,
Arek
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Arek,
If you calculate the average input current at your conditions, then you will see that you need to supply 2.4A continuously to meet that conversion ratio 5V to 12V at a 1A load. If you consider losses in the converter, that number is even higher. For instance, if the converter 90% efficient, you would need 10% more current at the input, so the average would be closer to 2.64A. Then, considering it is a switching converter there will be a ripple current causing the peak to be some percentage higher than that (maybe 3A peak current). Looking at the EC table of the datasheet on page 5, we can see that the current limit minimum value for the switch is 2.1A. The switch will see the exact peak current through the inductor which we know will be higher than 2.1A. Therefore, you definitely cannot use this device for this application at 1A.
-JP