We need to operate this at the maximum switching frequency of 1.6 Mhz as set by a resistor. There is no option in the web bench to change the frequency. It is set at 532 Khz or similar. Can this feature be implemented in the web bench for this part
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We need to operate this at the maximum switching frequency of 1.6 Mhz as set by a resistor. There is no option in the web bench to change the frequency. It is set at 532 Khz or similar. Can this feature be implemented in the web bench for this part
Hi, Sir
1. TPS56921's max Vout is 1.48V, it cannot support 1.65V output voltage.
2. For switching frequency setting, we should make the ON time of normal operation is larger than 150nS(minimum ON time.)
Supposed the application condition: Vin=12V, Vout=1.48V, IC only supports ~800kHz max frequency, so you cannot change it to 1.6MHz in webench.