This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63020EVM-487: Check TPS63020 output current capability?

Part Number: TPS63020EVM-487
Other Parts Discussed in Thread: TPS63020,

Hi Webmaster,

My customer was testing the TPS63020 for SSD power system.

Their system Vin=2.6V ~ 5V, Vout = 3.3V and Iout = 2A

When they are using TPS63020EVM and test under this condition, TPS63020 only have 3.3V, 1.2A output.

If we change loading to 2A, the voltage will drop to 1.5V.

When I configure the design setting into the Wenbench,  TPS63020 can drive 3.3V, 1.9A output.

My question is how to shorten the test gap with Wenbench simulation?

Regards,

David