The Vin is 12V-24V,Vout=40V, Iout=20mA.Working long hours,Vout occasionally droped to less than 10V,and the inductance(L1) is whistling.I change L1 from 6.8uH to 150 uH,The problem still exists.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The Vin is 12V-24V,Vout=40V, Iout=20mA.Working long hours,Vout occasionally droped to less than 10V,and the inductance(L1) is whistling.I change L1 from 6.8uH to 150 uH,The problem still exists.
Thaks for your reply.I haven't check the SW, VOUT waveform.I tryed to reproduce this problem,but LM5001 now working normally for about 24 hours. Is it possible that environment temperature or quicked
changed load caused this problem? 6.8uH/8A inductance(L1) and 150uH/500mA inductance(L1) now are all works well,we used 6.8uH/8Afor mass production,did we need to change L1for 150uH?