This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25896: BQ25896 with 3series NiMH battery

Part Number: BQ25896

Hi

I want to know whether BQ25896 may use to 3 series NiMH batteries? NiMH voltage is 3.6~4.35V = 1 li-ion voltage.

Thanks 

Star

  • Hi Star,

    When charging at <0.5C, it is generally acceptable to terminate NiMH using a safety timer only.  The BQ25896 can do this but the 4.2V default VBATREG and 2A charge current will need to be changed via I2C. 

    When charging at >0.5C , it is highly recommended for long battery life to terminate NiMH with either very precise dV/dt or dTemp/dt termination method, which the BQ25896 cannot do, even with host software and its 7-bit ADC.  A more precise ADC, controlled by the host, would be necessary to determine when to terminate.

     Regards,

    Jeff