This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62040: Protect

Part Number: TPS62040


Hi:

Regarding TPS62040, please help to confirm the following questions:
1. What is the mechanism of device short circuit protection?Is there a risk of triggering short circuit protection if the output terminal is too large?
2. After triggering the short circuit protection, will it be automatically relieved when the conditions are met?
3. As mentioned above, is there a maximum limit for the output capacitance?How many if any?
4. Is 1.2a continuous output current?