Tool/software: WEBENCH® Design Tools
Hi.
I need to design a universal input to 90V@5W isolated converter.
This converter must have a very low output voltage ripple, typically lower than 50mV and high efficiency higher than 85%.
It seems to be good to use LM5023 with flyback topology.
But in order to keep the converter in continuous current mode for lowering the output ripple , the inductance of transformers will be high and so transformer big.
And the maximum switching frequency of LM5023 is 130kHz, not so high.
Please help me how can I realize this converter optimally.
Thanks!