This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: Interfacing with BQ25703A

Part Number: BQ4050
Other Parts Discussed in Thread: BQ25703A, , BQ78350, BQ34110

Hello,

the BQ4050 is a SMBus device. Can it interface with the BQ25703A charger, which uses I2C?

There is a developmentboard (without documentation) available that uses these two devices:

http://www.ti.com/lit/df/tidrzn1/tidrzn1.pdf

Can you also recommend an I2C alternative to BQ4050?

BR,

Fabian