Hi,
I'm using the AFE chip BQ76940 for a 48V BMS system with the AFE configured as a 13S system. Out of the 45 boards we made, 4 to 5 boards worked fine for the first few hours, later on they developed an error in the measurement of Cell 5 voltage. Below mentioned are the voltages I've observed on the board.
- REGOUT = 2.52V
- Voltage of Cell5 before filter resistor R5 = 3.9V (That is the actual cell voltage).
- Voltage of Cell5 after filter resistor R5 = 3.43V (Hence there is a voltage drop of 0.47V across R5)
- Voltage drop across the diode connecting the VC5 to VC5X = 0.54V
- VC5X to CAP2 = 3.29V
- VC10X to CAP3 = 3.29V
- Voltage across the resistor (1kOhm) connecting Cell5 to VC5X = 0.84V
From the last point in the above design, the pin VC5X appears to be sinking around 0.84mA as opposed to the 25uA mentioned in the datasheet.
Kindly let me know how to address this issue. This issue hasn't appeared on the remaining 40 boards I have mentioned.
Thanks and Regards,
Bharath B