This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62130A: Is the TTPS62130A suitable for low-capacity design at the input?

Part Number: TPS62130A
Other Parts Discussed in Thread: TPS62135, TPS62136
My design conditions are as follows:

Vin=5.7V~ 8V

Vout= 5V

Iout=3A

Cin = Input capacitance can only be less than or equal to 9uF

Freq. = 1.2MHz or 2.5MHz

Working temperature = 60~70 degrees

----------------------------------------------------------------------------------------

Can such a design condition be applied to the TPS62130A?