This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: GPCRB report T Rise and T Time Constant is out of range

Part Number: BQ34Z100-G1

Hi

My customer follow the following steps to learning

Bq34z100-g1 with 8S1P cell. My test procedure is as bellows:

1. Room temperature test:

(1) firstly discharge the two batteries to 24V at room temperature and let them stand for 2 hours

(2) use the charger to fully charge the battery

(3) leave at room temperature for 2 hoursf

(4) put it in a 25-degree temperature box and let it stand for 2 hours

(5) discharge from 5C to 24V

(6) let stand for 5 hours

2. Cryogenic test:

(1) firstly lower the two batteries to 24V at room temperature and let them stand for 2 hours

(2) use the charger to fully charge the battery

(3) leave at room temperature for 2 hours

(4) put in a -10 ℃ temperature box and let stand for 2 hours

(5) discharge from 5C to 24V

(6) let stand for 5 hours

attached the data and report

HV3-0-8S-RB.zip

HV3-0-8S-RB-report.zip

From the report we can see T Time Constant 11464791, T Rise 738061.61 these parameters are too large and out of the register data range 0~32767.

Waiting for your reply.

Thanks 

Star