Dear Sir:
Under full load, the power factor is the highest at AC90V and slightly lower at 264V.
Under specific input voltage, full load power factor is the highest, light load will reduce it.
Could you tell why and explain the details?
Would you tell me if there is any correction plan that can meet the requirement of high PF value even under light load?
Thank you very much.