Other Parts Discussed in Thread: EV2400
Greetings,
We're working with the BQ2520AEVM (Evaluation Board) interfaced with the EV2400 and Battery Management Studio v1.3.86. It is attached to both a 4.2V LiPo battery (VBat) and a power supply (VIn). We also attached a simulated load to the VSys. We noticed a couple issues.
1.) If there is no load present on VSys and VIn is removed, VSys goes from 1.8V to 3.0V. What is the minimum load for a stable output on VSys? Is there a minimum load on VLDO as well?
2.) During our testing we found that the Battery Management Studio only reports "Device ACK OK" when the charging voltage is present on VIN. Looking at the schematics, the I2C lines should be pulled up to VSys, not VIn. Does the I2C communications require VIN? Could it be a limitation of the EV2400 I2C interface?
Thanks!