The PG pin pull up to the 3.3V_ASIC by 1M ohm resistor then connector to the other TLV62085's enable pin. When the temp is lower about 70 degree it is work,
When The temp higher over 70 degree the PG pin's voltage only has 0.9V. (3.3*400k/1400k.) It's 3.3V_ASIC output is still correct 3.3V but PG signal could not push the the next power IC.
I need to reduce the 1M ohm to 10k or 100k that it can work normally.