Hi,
I'm trying to read the ADC value in Active Battery Mode. Although, I can read the I2C register but the value (Vts, Vbat, Vin, etc.) don't change.
I have set the ADC_READ_RATE to 1s (Address 0x40 <--0x82) and the LP pin is high (~2V). When I set the ADC_CONV_START bit high, it is directly set back to 0 so the conversion should be completed, but I cannot see any change in the data value. (Even if I modify Vts by changing the trimmer value.)
Did I miss something to enable this reading ?
Best Regards,