This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS650864: TPS6508641 or TPS65086401?

Part Number: TPS650864

Hi

Our customer uses Zynq UltraScale+ MPSoC.
The attachment  file is a power estimate calculation.
Which way of TPS6508641 or TPS65086401 should the customer use?

FPGA_Power_pwr.TXT

Regards,

PAN-M

  • Hi PAN-M,

    For a ZU2CG design with max current of 2.1 A, it mostly depends whether a 5V rail is desirable or not. If not, the TPS65086401 is likely more preferable (less rails used so fewer external components). For these low currents,TIDA-01480 is also an option if they prefer 5V input design.

    I'd also like to add that if they want to customize their design, the TPS650861 is also available which is a fully programmable version of the TPS650864. It offers OTP Generators that are already pre-filled out to match the TPS6508641 and TPS65086401 so that quick editing is possible.

  • Thank you for suggest.
    Please wait for the result because I contact our customer.

    Thanks and Regards,
    PAN-M