Other Parts Discussed in Thread: CSD18563Q5A, , CSD18537NQ5A
Hi Team,
My customer did a design following our LM25116 Evaluation Board but did some change on BOM. Their target input,output is almost the same as our EVM, [7-42V input, 5.1V 7A output], I have done the first round check. below is the difference, please help to comment if some potential issue. thanks.
1. Different divider resistors at FB 【pin 6】,they used 5.1k and 1.6k, but ref design is 3.7k and 1.21k
2. R11 between Vout and VCCX, does this need or not?
3. An extra capacitor C31 between CS and CSG
4.An extra 0Ω resistor at HO AND LO pin.
5. Different inductance, They used 9,2uH,but ref design is 6uH
6.Different MOS, They used our CSD18537, but ref design is SI7850.
EVM link: