Hi
My customer has question.
The data sheet specifies DAMX under the following conditions.
RON = ROFF = 75kΩ
RDRL = 10kΩ
DMAX = 66% -74%
If the same conditions are used and calculated using equations (1) to (5), DMAX ≒ 65%.
There is a difference of 5% compared to the standard value TYP.
Is this correct?
Best Regard
T Kishi