This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24160: Clarification on STAT_x bits of BQ24160

Part Number: BQ24160

Hello,

Currently I'm using BQ24160 in one of my designs. In status/Control Register, there are two indications in STAT_x bits, those are unclear to me.

000 - No valid source detected
110 - NA

What is the difference between these two?

  • Hi Kasun,

    For 000, the charger checks the input source at power up by pulling a small current.  If the voltage at IN/USB collapses, the charger disables that input and reports No valid source detected.

    For 110, that fault state is not used.

    Regards,

    Jeff