This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54360B-Q1: DC DC converter

Part Number: TPS54360B-Q1
Other Parts Discussed in Thread: LM76003-Q1, TPS54360B, LM76003

Hi Team,

I have a requirement for DC DC converter for automotive grade requirement,

DC DC converter will be driven through a vehicle battery, which is 12.6V [TYP]

Vin: 12V ~ 60V  [Range]

Vout: 5V

Iout: 3.5A

I build a circuit through webench power design tool and found, "TPS54360BQDDARQ1 " this part. Please find the attached schematic for your reference.

Here is my clarification, am i selected the right part for my requirement ?

Do we have any other better solution to my requirement, where my circuit blocks are having below peripherals 

GSM, GPS module, Micro Controller, 3.3V LDO, Battery Charger [4.2V], 3.8V GSM regulator, USB-Serial converter, RTCSCHEMATIC1 _ Power Block.pdf

Thanks,
Rahul