I have a design where I need to supply power to a high load PWM-like device.
Input is 45-50V, output is 24V.
The load is a pure resistive load that can vary between 1-1000 ohms, and is pulsed with a period of approximately 1ms, with a duty cycle of max 65%.
The load can vary from one pulse to another between the extremes (1-1000 ohms).
The target is an industrial application with long life time support needed, so long life components are needed.
Any recommendations?
/PA