This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZ12003: LMZ12003TZX-ADJ/NOPB

Part Number: LMZ12003


Hello

I want to use LMZ12003TZX-ADJ/NOPB part to generate 5V @ 2A from 7V input.

But when i a, giving the above input at Webench it says design can not be created.

Is there any limitation with the input voltage as when i change the input to 8V design is created.

Regards

Akash Jain