This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61220: Switching current limit

Guru 16770 points
Part Number: TLV61220
Other Parts Discussed in Thread: TPS61220, TPS61099

Hi

Our customer has following requirement for boost converter.

Vin = 2V to 3V

Vout = 3.3V

Iout = 100mA

Surface mount package

According to datasheet of TLV61220, minimum switching current is 200mA.
Additionally, output current is limited below 90mA for our input range due to minimum Isw shown in Figure 2.

It might be the same as TPS61220.

Is it difficult to use TLV61220/TPS61220 for the customer's usecase?

BestRegards