This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74700-Q1: When will recover back if meet reverse current protection

Part Number: LM74700-Q1


Hi team,

There is a description in datasheet as below, to double confirm, is that mean when LM74700-Q1 in reverse current protection, it will recover back to turn on the MOSFET once Vin-Vout > 50mV?

A fast comparator shuts down the Gate Drive through a fast Pull-Down within 0.45 μs (typical) as soon as V(IN) – V(OUT) falls below –11 mV. It turns on the Gate with 11mA gate charge current once the differential forward voltage V(IN) – V(OUT) exceeds 50 mV

Thanks.