This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Possible Bricking of bq20z95, what commands could bring it back?

Other Parts Discussed in Thread: BQEVSW

I was messing with the BQTester V1.0.2, which doesn't have support for the BQ20z95 built in. I read somewhere to add it in the targets folder so I did. Then I attempted to upload my golden dfi, then golden .rom file to my board. 

 

I believe I have put the IC into some sort of rom mode. I can't seem to program it with the bqEVSW, or read SBS data from it. I get a vb_t2h_unknown error from the sbs screen when trying to scan. What are some commands that I could shoot over to the IC that might revive it? Any and all thoughts would be greatly appreciated.

 

Thanks,

JD