Other Parts Discussed in Thread: TPS3613-01,
Hello,
I am using the TSP3606-33 IC in a battery powered design. For my design the part's Vdd is connected to a 3.3V regulated supply that is derived from a main battery pack. My application has a secondary "backup battery pack" that is regulated down to 3.3V as well. This regulated battery backup is connected to the part's Vbat pin. I want the TSP3606-33's Vout to switch to the regulated Vbat source when the Vdd pin falls just below 3.3V.
Page 5 of the datasheet has the following statement "Vbat only connects to Vout (through a 2ohm switch) when Vout falls below Vswn and Vbat is greater then Vdd." I read in the datasheet that Vswn is typically 2.93V + 2% which is ~2.98V. So this would seem to indicate that the part will not switch until Vout < ~3V. The behavior I am seeing with my design is that Vdd must fall to < 3.0 volts in order for the switch to occur which agrees with my understanding of the datasheet. This however is problematic for my design because Vout from the TSP3606-33 IC powers circuitry that requires ~3.3V.
So I want the TSP3606-33 IC to switch when Vdd falls just below 3.3V. I am not clear how this part can achieve this behavior however. I am happy to share my application's schematic if that would be helpful.
I appreciate any help possible.
thank you.
-Sean