This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL431: Stability boundary conditions against load capacitance(TL431A)

Part Number: TL431


Hi Application team,

My customer is using TL431AIPK in an application and ask us the stability conditions against load capacitance.

On page-17 in TL431 datasheet(SLVS543P) , there is a graph(Figure-16) showing the stability bundary condition against load capacitance. But this graph is only for 25degC and customer would like to have the boundary conditions over recomended temperature range(-40 to 85degC) to judge the stability of their TL431A application circuit.

- Can you show the similar boundary graph at other low and high temperature based on IC recommended temperature range?
- If the boundary data( or graph)  is not available, How can they judge that stability on TL431A application over customer's use temparature range?

Regards,

H.Someno