This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: Capacitor selection

Part Number: TPS1663

Hi,

I'm designing a PCB based on TPS16630REG. My requirements are

Input Voltage : min - 4.5V max - 5.5V

Input Current: 5A

Output Voltage : 5V

Output Current : 5A

How to choose Cout and Cin capacitor for my application? Is there a equation for that? 

Regards,

Vijan