This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL4242: QUESTION OF PWM DIMMING

Part Number: TL4242

HI,

     I am testing TL4242, find the PWM dimming not work.

    12V power supply
It was found that PWM PIN > 1.3V, LED was fully bright.
PWM < 1.3V, LED is completely extinguished and has no dimming function.
Where is the problem
?

    my schematic diagram as below:

thanks,

  • Hi, YISYUAN,

          Please note that high level of PWM enables the device and low level disables the device.You can regulate the LED brightness through the duty cycle of PWM rather than the amplitude of PWM. I suggest that you should first read the datasheet carefully.