This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LM5122-Q1: Hi, I have a question about boost converter webench simulation.

Part Number: LM5122-Q1

Tool/software: WEBENCH® Design Tools

Hi,

I used lm5122-Q1 for webench boost converter simulation.

I got a pretty good result about inductor current.

However, In switching voltage graph above, i got the peak voltage.

I wonder why there is peak voltage from 24V to 25V.

Did it happen because the circuit is not stable?

Thanks,

Best regards,

Yunsik