Other Parts Discussed in Thread: EM1402EVM, SN74AHC595
Hi
I am using the EM1402EVM and the example control software that TI provides.
I was wondering if RCLK on the SN74AHC595 must be toggled or the line can be left high to still ensure the data is clocked in. It appears to be left high in the example code.
Also with respect to the SN74AHC595 it states, in the datasheet I have, that fmax has to be a minimum of 85MHz. Does that mean that the RCLK and SRCLK have to operate at a minimum of 85MHz. This is far from the frequency that the sample software would be able to clock the data in.
Just wanted to get clarification
Thanks,
Malcolm