This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1663: TPS16630 Low Current Shutdown Control

Part Number: TPS1663

Hi,

I'm designing a PCB based on TPS16630REG IC.

My requirements are 

Input and output  Voltage - 5V

Input and output Current - 5A

 

My question is how to connect Low Current Shutdown Control  Pin (TPS16630 Evaluation board connect this pin to button). Is it OK if I leave Low Current Shutdown Control pin  as a floating?.


regards,

Vijan