Other Parts Discussed in Thread: TPS62826, TPS62090
Hello,
I need a buck regulator with 2.5V input and 0.8V output.
The TPS62088 can be a choice, but it is not automotive qualified.
Is there a plan for AEC qualification of this device or similar devices like TPS62826?
I have seen the TPS62090 which is automotive qualified, but min. input is 2.5V.
What can happen if my input would be something like 2.4V?
Best regards,
Michael.