Dear All:
I design the 17S BMS with BQ76930, In my application, when the BQ76930 is wake up, the regout can output voltage, I use the REGOUT to enable the system DC-DC IC EN pin, I find the Regout would be
pull down immediately as shown in the following figure. can , if i disconnect the Regout from the DC-DC En pin , the regout output is normal. can you help me to solve the problem, Thanks