Other Parts Discussed in Thread: LM5576, PMP10812,
Hi,
I have referred PMP10812- Class 2 Non-isolated PoE Buck Converter (5V/1A) Reference Design.
http://www.ti.com/tool/PMP10812
http://www.ti.com/lit/df/tidrtg6/tidrtg6.pdf
But my design requirement is 24V/0.5A output.
I have designed DC-DC buck converter with IC- LM5576 for 30-60V input and 24V/0.5A output using Webench utility.
Can I use PMP10812 reference design with an above DC-DC converter to make my board POE enabled?
If Yes, what designing parameter should I consider while using IC- LM5576 design with the PMP10812 reference design.
If no, why?
Your early replay most appreciated.
Thanks and regards,
Mishra.