Our customer is designing a 400W SMPS.
UCC256303 will be applied. Please review the circuit diagram below.
Additional questions
1) I don't want to use 8 pin BW terminal. Is there a way to disable?
I have a separate OVP circuit on the secondary side, so I don't want to remove the auxiliary winding from the primary transformer.
2) In the demo board, 2 resonance caps are used. Ref. I'm curious about the role of CM4.(What is the side effect if you delete CM4?)
3) In the guide data, Lr and Lm were used separately when designing the resonant transformer.
Should I design separately? Or can it be used as a general section type 1ea?
4) Is it possible to design 1KW?