Dears,
As SPEC in the 9.3.2 Input and Output Logic Table on page 21 of the Technical Manual, the DT pin should be directly connected to the VCCI. The INA and INB should be independently controllable. When the input is high, the output should also be high, but in the actual measurement. When both INA and INB are high, the output of both channels is low, that is, the logic of DT connected to VCCI in the truth table cannot be realized.
During the test, the voltage of the DT pin was paid attention to. The measurement was about 0.8V when connected to RC, and about 4.98V when connected to VCCI. In addition, in the circuit design, the DIS pin is grounded to a 10K resistor, and the resistance is always present during the test. And when the input INA and INB are not high, the output logic is the same as the input, in theory the chip can work.
Please help me to determine the reason why the logic can not be achieved.
Thanks!