Hi,
How can I move from the charged state to the charging process again?
Please tell us about each case when HZ_MODE = 0 and HZ_MODE = 1.
best regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
How can I move from the charged state to the charging process again?
Please tell us about each case when HZ_MODE = 0 and HZ_MODE = 1.
best regards
Hi,
The charger will automatically start recharging once the battery discharges below the recharge threshold (VRCH=120mV). Alternatively, you can force recharge by toggle the CE bit, HiZ bit or /CD pin. If a load transient on SYS causes a supplement event (battery must provide some of SYS load current), charge is also restarted. Removing/replacing either IN/USB or the battery also restarts charge.
If HZ_MODE= 1 or /CD pin = high disables the buck converter and places the chip in the lowest quiescent current state, with BAT tied to SYS through the BATFET (i.e., the battery provides the system load).
Regards,
Jeff