Other Parts Discussed in Thread: UCC28056, UCC28C42, UCC28881
hi Team:
I want to designed power solution:
Vin:85-265VAC
Vout:12/7A -85VDC/2.3A
could you pls help to Recommended solutions?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I think this might be a 3 stage solution.
1. UCC28056 critical conduction mode PFC design for 85V to 265V RMS to 390V output.
2. A UCC28C42 in a two switch forwarded to step down the 390V to 100V DC.
3. A UCC28C42 setup in a buck converter to step down the 100V DC to 85V to 12V DC.
4. It might even be worthwhile having a little offline buck converter using the UCC28881 to regulate the IC power to the two UCC28C42 devices; as well as, the UCC28056.
Regards,