This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

18650 Battery management system design

Hello, could somebody suggest a reference battery management system design?

My application requires the following:

-3 lithium 18650's in parallel

~5.5 V output voltage

-Continuous draw will be ~1 A but could have a short peak of up to 1.6A

-Charging circuit. I have not determined the input/charge voltage but if it were also ~5.5V then that could simplify
the circuit.

I need the following from a battery management system:

-State of charge (SOC) analog output

-Charging or not charging digital output

-Status/trouble flag digital output

-Overcurrent/overvoltage protection