hi there!
I would like to use the BQ25713 to manage a NiMH battery pack (6 cell, ideally!)
your selection table shows this part as suitable for all sorts of chemistries including NiMH, but the datasheet seems to infer the only cells it will work with are Li-Ion.
Looking at the basic battery voltage and current specs for the part this shouldn't be a problem, but as NiMH obviously has different requirement to Li-Ion, I would like to understand any issues around doing this and what is needed to make the system work..... but there seems to be no info in the datasheet and no application notes I can see to discuss it.
failing this, I'll have to go with LTC4010.. at least I can see that will work... even though it's quite primitive and doesn't really have all the features I'd like.