Dear Sir,
We are going to use TPS2121 power mux IC for power switching purpose.
Schematic Diagram is attached.
Our system is Battery operated system.
Battery voltage = (4 x AA Cell Battery) = 6V
Normally system will run on Battery.
But in case of Low Battery or Battery is removed, then system should operate on 5V USB power supply.
If Battery is present with good health & USB power is applied then
system should operate on USB power supply to save Battery Life.
So, our first priority power supply is USB power supply.
Design detail is as follow.
1st Priority power supply = 5V USB power = IN1
2nd Priority power supply = 6V Battery = IN2
Over voltage protection = disabled for both power supply
My questions regarding this design are as below.
1) During power on the system, if IN1 supply is not present(USB power supply is not applied),
will system start directly from IN2 power supply (Battery), or
It is compulsary to start the system first from IN1 & then it could switch to IN2.
2) I am clear about Status Pin (ST) functionality.
But I am not clear about Status Pin (ST) output voltage specification.
If this pin is open drained? So, that I need to apply pull up resistor.
Or
It gives high or low logic output just as simple GPIO.
If yes, then what will be the output voltage at logic high? is it 5V or 3.3V?
3) What are the maximum values of resistor (R1 & R2) I can apply to save power?
(i.e. (1M & 1M range),(100K & 100K range),(10K & 10K range) )