UCC28070 IPFC CONTROLLER IC
PICTURE 1) THIS IS A CAPTURED SIGNAL OF PIN #1 (USING THE STOP FEATURE OF THE OSCILLOSCOPE) FROM PIN #1.
PICTURE 2) THIS IS THE SAME WAVEFORM AS PICTURE 1 AFTER I CLICKED THE HORIZONTAL OF THE SCOPE.
PICTURE 3) THIS IS A CAPTURED SIGNAL OF PINS 14 & 17 (USING THE STOP FEATURE OF THE OSCILLOSCOPE).
PICTURE 4) THIS IS THE SAME WAVEFORM AS PICTURE 14 & 17 ( AFTER I CLICKED THE HORIZONTAL OF THE SCOPE).
THESE ARE THE ONLY THREE PINS THAT ARE ACTING THIS WAY. I HAVE USED THE TRIGGER ADJUSTMENT, BUT THESE SIGNALS WOULD NOT CHANGE.
QUESTION 1) HAT WOULD CAUSE THESE MULTIPLE SIGNALS TO APPEAR?
QUESTION 2) WHAT PIN NUMBER(S) ARE ASSOCIATED WITH THESE SIGNALS?
I NEED YOUR EXPERT ADVICE ON HOW TO RESOLVE THE ISSUE.
LOOKING FORWARD TO YOUR RESPONCE.